This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB933-Q1: 请问DS90UB933匹配DS90UB962做360全景,DS90UB933匹配DS90UB962做360全景,30帧和25帧外同步怎么设置。

Part Number: DS90UB933-Q1


请问DS90UB933匹配DS90UB962做360全景,DS90UB933匹配DS90UB962做360全景,30帧和25帧外同步怎么设置。

  • 已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 您好

    您能否澄清933和962匹配的含义? 是否要将帧同步信号从反串行化器转发到成像器? 请注意,帧同步的目的是同步多个成像器,而不是同步SerDes本身。

  • 外同步的目的是同步多个成像器,解串器配置外同步25帧或30帧通过链路反向传到摄像头的933的同步输入,然后通过933的输出脚输出同步信号到sensor的同步信号的输入脚,就想知道解串器的外同步信号怎么配置(我们现在是用933的15脚(GPO-0)作为外同步信号控制脚

  • 您好

    要编程962解串器以接收外部帧同步信号,请根据所需的GPIO引脚对寄存器0x18[7:4]进行编程以接收信号。为了对962解串器进行编程,使其通过反向信道将帧同步信号发送到933串行器,请根据所需的GPO信号对寄存器0x6E或0x6F进行编程,以在串行器上输出。最后,为了对933进行编程以输出帧同步信号,根据所需的GPO引脚对寄存器0x0D或0x0E进行编程,以输出信号。

    对于933上的GPO0,请特别使用以下设置:

    962-0x18[7:4]取决于所需的GPIO引脚来接收外部信号

    962-0x6E=0x8A

    933-0x0D=0x55