This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848I: DP83848IVV 100MHZ 速率配置可以与电脑通讯,配置10MHZ 不能通讯,

Part Number: DP83848I


DP83848IVV  100MHZ 速率配置可以与电脑通讯,配置10MHZ 不能通讯,测试10MHZ时TX及RX的差分对信号,信号波形与100MHZ时类似,但是频率不对,请问这个是什么原因?

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 1.板子程序自动协商,电脑这边自动协商及100MHZ可以通讯,电脑设置成10MHZ不能通讯。

    2.板子程序设置成100MHZ,电脑自动协商及固定100MHZ可以通讯。

    3.板子程序设置成10MHZ,电脑自动协商不能通讯,电脑设置成10MHZ可以通讯上。

    板子程序设置成10MHZ,测量TX差分对信号,波形与100MHZ时类似(此时电脑以太网速率自动获取,电脑端显示在100MHZ查询),经手动将电脑端速率改为10MHZ,测量TX差分对信号与手册里类似,可以通讯上,但是电脑与其他设备通讯,电脑自动协商,其他设备设置成10MHZ,是可以协商后通讯上的。

  • 确保DP83848的自动协商相关配置正确。

    检查原理图和PCB布局,确保符合10M要求。

    以上都可以对比参考官方开发板进行。

    另外,可以更新电脑网卡驱动试一下。