This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM26LV31: 与输入引脚连接管脚容易被烧短路

Part Number: AM26LV31

您好!

    目前遇到的问题是:

1、在1A引脚出外部上拉一个1K,上拉电压是3.3V,然后在连接到FPGA 逻辑控制IO口,电平都是对应的3.3V,但在正常使用过程中偶尔出现,该逻辑IO会对地短路。

2、使用万用表查看AM26LV31IDR的1脚位和GND没有对地短路。

该引脚短路。麻烦大家帮我分析下。我的连接关系如下。

我分析的原因可能是该芯片的VCC电压超过了所规定的Operation  Conditions中的3.6V,但未超过Absolute Maximum Ratings中的6V,故有点这方面的因素。