Hi team:
If my design does not require the use of VEXCC and only needs VCC1 and VCC2, how should the VEXMON, VEXCTRL, and VEXCC pins be handled? In the schematic design, can they be left floating? If left floating, what issues might arise?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team:
If my design does not require the use of VEXCC and only needs VCC1 and VCC2, how should the VEXMON, VEXCTRL, and VEXCC pins be handled? In the schematic design, can they be left floating? If left floating, what issues might arise?
If VEXCC is not going to be used in application then you need to do the following:
1. Short VSUP to VEXMON - don't add a 1ohm resistor - it should be shorted.
2. You can leave VEXCTRL floating
3. You can leave VEXCC floating
The rest of the schematic - from what is shown - looks okay. Please remember to put 100nF decoupling caps as close to the power input pins as possible. They also aren't showing the reverse polarity blocking diode and I'd suggest they add that - if they haven't already (it might just not be shown in schematic). You may also want to add a little more capacitance on the VSUP pin for EMI reasons.
Please let me know if you have any questions!
Thanks for your reply. But in my first use, if I use VEXMON VEXCC for functional debugging, a sampling resistor connect VEXMOC and VSUP.However, during mass production of the final solution, I may not use VEXCC. Therefore, VEXMON and VSHUP cannot be shorted directly. I can only replace the sampling resistor with a 0R component and leave other pins floating. Would this approach be feasible?
That should be okay - if you may use it during test/debug using a 1 ohm resistor is fine - just be sure to keep VEXCC disabled during production builds.