Part Number: ISO1228
在SINK/SOURE共源模式下,SINK跟SOURCE二次側動作H/L為相反的。
請問有什麼方法可以讓動作H/L相同??
或是讓MCU知道當下輸入源為SINK或SOURCE??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes, the H/L would be opposite if in SINK or SOURCE mode.
Both Sink and Source modes will output a high when 24V is seen across the INx and LEDx pin. When the sensor is CLOSED the corresponding OUTx will be HIGH. Therefore, no inversion will be needed.