This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1042: Do TI have the chip to isolate CAN_H and CAN_L?

Part Number: ISO1042

As we know, ISO1042 us a chip to isolate between can_tx can_rx and can_h can_l. 

Now we want isolate can_h and can_l directly.

Do TI have the chip to isolate CAN_H and  CAN_L?

Now out problem is below:

We have only one can controller,so we only connect one can transceiver at can controller by can_tx and can_rx. Now we need connect two device at can transceiver by can_h and can can_l, and two devices,can transceiver should be isoltated each other.

So we need the chip to isolate can_h and can_l.