This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOW1432: 关于多个ISOW1432重叠放置的PCB Layout问题

Part Number: ISOW1432

我现在在做一个8层通信类的印制板,使用了多个ISOW1432,不同的ISOW1432的总线需要连接到同一个连接器上,每个器件包括A,B,Y,Z,GND,一共5线。布局方面印制板上空间有限,422芯片只能两两重叠放在L1和L8层。

请问在A,B,Y,Z侧:L2层使用GND(422L1)平面,L4使用Viso(422L1)平面,L5使用Viso(422L8)平面,L7使用GND(422L8)平面,这些在垂直方向上是完全重叠的,这种方法推荐吗?还是有更好的方法?

由于走线空间限制,我无法保证L1和L8的ABYZ在垂直方向上不交叉或完全分隔,事实上现在他们在垂直方向上是平行重叠的。