尊敬的TI工程师,
您好!
1.请问GND2需要引出来,和CAN总线上其他设备的CGND连到一起吗?
2.我设计的电路板上的所有的地都是一个地,CGND2需要接电路板的地吗,我对于CGND2接到哪里很困惑。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
1、由于 CAN 是一个差分接口,如果CAN总线只连接了 CANH/CANL两根线,只要 CAN 线路与接收 CAN 节点的总线侧接地有关的共模电压处于其建议的工作条件内,整个网络将工作正常。 但是在嘈杂的系统环境下,最佳做法是使用第三条接地参考线,并将其连接到所有节点。这样,每个 CAN 节点的接收器都有一个参考,不会超出共模电压范围。因此,是建议将ISO1042的GND2通过一根线与CAN总线上其他设备的CGND连到一起的
2、因为ISO1042是隔离CAN收发器,其VCC1和VCC2、GND1和GND2是隔离的,因此VCC1和VCC2供电是需要隔离的,GND1和GND2也就不能连接在一起,但是看到您VCC1和VCC2并没有使用隔离电源而是使用的同一个电源,或者说您并没有使用ISO1042的隔离功能,那么就需要将GND1和GND2连接在一起
VCC1和VCC2分别用不同的5V电源供电
这里不同的5V电源,那么两个电源隔离了吗?如果隔离了,那么隔离电源VCC2就需要将去耦电容接在隔离地GND2上;如果没有隔离,那么就没有隔离作用