Part Number: ISO1042
canl和canh是3.3v供电,能否转成5v供电的rx和tx呢,二者如果电压不同,会出现错误吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,VCC1的电压范围为1.71~5.5V的电压范围,所以VCC1可以是1.8V,可以是3.3V或5V,但是VCC2的电压范围为4.5~5.5V范围,所以VCC2为3.3V是不允许的。