This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

低压直流隔离电压采集方案?



要采集光伏电池的电压(0~25V之间),隔离降压到0~3.3V供给DSP的A/D采集,随后实现最大功率点追踪算法。

我想到的方法:(1)非线性光耦,例如PC817、EL357等,要做分段线性,精度远远不够。排除。

(2)线性光耦,例如HCNR201,光耦输入端要用运放做线性补偿,该运放需要电源,该电源需要设计buck降压电路实现,电路太冗余繁复,暂时排除。

(3)霍尔电压传感器,精度不够,排除。

所以这个问题如何解决呢?第一,一定要隔离,我用的拓扑结构,光伏电池的负极与单片机不共地;第二,精度尽可能的高;第三,电路尽可能的简单;第四,成本尽可能低。