This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7341FC: 用ISO7341FCDW 替代 SO7241CDW 在RS485接口上测试时 出现3%的数据丢包? 原型号就不会这是为什么呢?

Part Number: ISO7341FC
Other Parts Discussed in Thread: SN65HVD75, , ISO7241C, ISO7341C

你好!

   产品原始使用的数字隔离器型号是 ISO7241CDW 接口是RS-485 最大通信数据是57Kbps, 负载是PLC,使用  ISO7341FCDW做替代测试时 发现有3%的丢包率。看了规格书 ISO7241CDW 和 ISO7341FCDW 最大通信数率是 25Mbps,应该不会有数据丢包问题 且 ISO7241CDW 使用没有问题,咨询过线上技术说 ISO7241CDW  和ISO7341FCDW 都不适合用于RS-485通信,请问这是为什么呢?  查询过 SN65HVD75 的规格书 有推荐ISO7241 使用RS-485电路。