Part Number: ISO6760L
Other Parts Discussed in Thread: ISO6760, ISO224, AMC1311
你好,请问数字隔离器可以传输模拟信号吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,ISO7x,ISO6760系列的基本上都是数字隔离器,用来隔离数字信号的。
不知您具体是什么应用,如果需要隔离模拟信号,可以参考ISO224或者AMC1311。
您可以参考下AMC1311的数据手册,这款隔离放大器的Gain=1,0~2V的输入电压不知是否满足您的需求: