Part Number: ISO1430
工程师你好,
通过查询资料,发现RS422与RS485的电气要求基本一致,请问RS422的Y、Z与A、B,是否建议与RS485一样,需要增加上下拉电阻?
即:Y与A需要上拉至VCC,Z与B需要下拉至GND
多谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,AB上下拉并不是485必须的,而是因为有些收发器内部没有失效保护电路,当总线处于短路或者空闲时,将总线处于一个固定的逻辑状态,所以A上拉,B下拉。
但是我们的485收发器很多内部集成了fail safe保护电路,所以AB外部是不需要上下拉的。
同样对于ISO1430来说也一样,内部集成了失效保护电路,所以外部不需要上下拉。