This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO3088: CPU侧RX下拉,发现通信异常

Part Number: ISO3088


 ISO3088 CPU连接侧RX与TX是否需要上下拉处理,目前RX做下拉处理,发现通信异常。RX和TX信号是否需要上下拉处理,是否有设计方案

  • 您好,

    RX不需要下拉电阻,RX是 ISO3088输出管脚,RS485接收器始终在驱动该引脚;

    TX是ISO3088输入管脚,看主控端管脚的输出类型,如果是推挽输出,则不需要加上下拉,如果是OD或OC输出,则需要加上拉;另外,当主控端会存在输出不确定电平时(比如当主控端复位时,会将其I/O引脚配置为高阻抗输入),TX建议加上拉,以防止在此期间,TX管脚电平不确定,导致总线传输噪声信号。