Other Parts Discussed in Thread: ISO1042, TVS1401
现场多次出现ISO1050DUB收发器损坏,前端的TVS正常,原理图如下;能否帮忙分析一下可能的原因,谢谢。


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
电路图中NUP2105L TVS管不能保护 ISO1050,VCANH or VCANL能够承受的电压是–27V~ 40V,而NUP2105L 的钳位电压(maximum clamping voltage)大于VCANH or VCANL能够承受的电压。请查看下面链接的文档,了解如何正确保护ISO1050:
https://www.ti.com/lit/an/slla419/slla419.pdf?ts=1588081931616

看下面NUP2105L datasheet截图,其钳位电压与脉冲电流峰值有关,如果应用的环境比较良好,不会有太大的浪涌脉冲,钳位电压就会比较低,那么这个应用可以起到保护作用;如果环境比较恶劣,浪涌脉冲比较大,那么钳位电压就会比较大,超过总线承受的耐压,那么对ISO1050就起不到保护作用。
但这个截图给出的最小钳位电压是31V左右,而ISO1050的VCANH or VCANL能够承受的电压是–27V~ 40V,这很说不过去,这里应该有误,我会向相关负责人员反馈下这个问题以文档进行修改。
这里建议您重新选择TVS管,或者将ISO1050换作ISO1042,ISO1042的VCANH or VCANL能够承受的电压是–70V~ 70V,然后再看下在现场应用中是否还会发生故障。

您可以使用上述链接中推荐的CPDT-12V (VBR = 13 V)
看下面链接CPDT-12V datasheet,它满足防静电空气15KV要求。
https://pdf1.alldatasheet.com/datasheet-pdf/view/315542/COMCHIP/CPDT-12V.html