Other Parts Discussed in Thread: THVD1400
工程师你好,
我在阅读ISO1412芯片规格书时,发现在这款全双工RS422芯片中,依然设置了RE与DE管脚。
1.请问这样设置的目的是为了方便用户进行半双工输出么?即用A连接Y,用B连接Z,然后进行双线半双工RS485输出?
2.在此连接下,接口防护参数设置是否和普通的半双工RS485芯片(如THVD1400)输出一致?
感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.请问这样设置的目的是为了方便用户进行半双工输出么?即用A连接Y,用B连接Z,然后进行双线半双工RS485输出?
可以这么理解吧,这样既可以全双工,也可以将AY, BZ接起来就是半双工应用。
14xx其他系列比如1410,1430或1450的只支持半双工如下面架构图:
.在此连接下,接口防护参数设置是否和普通的半双工RS485芯片(如THVD1400)输出一致?
您指的TVS防护吗?是一致的,因为都是遵循的485协议, 共模电压范围-7V~12V,那么在选取TVS时的参数要保证TVS的stand off电压Vwm>12V.
或者您也可以直接参考隔离485收发器的设计指南:
RE低有效,所以当RE=L时,receiver enable。如果为高或者悬空处理的话,则disable receiver。
同样DE高有效,当DE=H时,driver enable,如果为低或者悬空处理的话,则disable driver。