This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7742-Q1: How to implement IIC communication using isolators

Part Number: ISO7742-Q1
Other Parts Discussed in Thread: ISO7742, ISO1540-Q1, ISO1541-Q1, , ISO7731

Hello,

     we are currently designing the IIC isolation interface circuit, and we plan to use ISO7742 to realize our scheme. We supply 5V power on the MCU side and 3.3V power on the slave side, may I ask how we should use this circuit?

    Does SCL1 and SDA1 match MCU or slave?

  • 您好,

    这里是中文论坛,您可以使用中文发帖。

    您是需要汽车级的I2C隔离器件吗?建议您看下 ISO1640-Q1ISO1540-Q1、ISO1541-Q1

    ISO7742-Q1不能应用中I2C通信中,因为I2C的SDA信号线需要是双向通信的接口,它有应答位。而ISO7742-Q1 四路接口都是单向的。

  • 我现在需要一款IIC隔离器,需要满足PIN 爬电距离满足≥10mm,ISO1640-Q1ISO1540-Q1、ISO1541-Q1这三款不能满足,可以用上图的拓扑电路使用7742完成IIC  SDA双向通信,我的疑问是这块拓扑电路,左侧接MCU还是右侧接MCU侧,有什么区别吗,感谢

  • 左侧接MCU,因为SCL是单向的,只能从左到右传输,而发出SCL时钟的是主控端。

    上述电路是实现SDA的双向通信,因为I2C的SDA是双向通信,SCL是单向的,而ISO7731的接口都是单向的,因此需要为SDA线路使用外部器件实现双向通信功能。如果系统是多主总线系统(两条线SCL和SDA都必须为双向的),那么SCL线路也需要用下面外围分立器件搭建。

    请注意上述电路会增加传输延迟。