Part Number: ISO3086


电路图 和参考芯片资料
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,接收端差分信号我看您这边上下拉R1和R647Kohm,并且终端匹配电阻R3=12Kohm。
首先RS422或485的终端匹配电阻Rt=120ohm。其次建议上下来电阻1kohm~10Kohm吸收噪声电流。
将这几个电阻阻值更改下试试。
抱歉,我上面说的上拉1Kohm~10Kohm指的是使能端,即RE和DE端。AB差分线的上下拉阻值是为了接收端建立合适的偏置电压。
ISO3086的数据手册我看了下,接收端已经集成了失效保护电路(也就是内部已经有偏置电路了),即总线在开路,短路,以及空闲时都能保持有效的逻辑状态,防止通信出现乱码,所以AB端是可以不使用上下拉电阻的。

另外,我想您可以将上下拉47Kohm阻值去掉,然后终端匹配电阻改为120ohm。按照您上面的拓扑结构,在最远端的收发器处端接120ohm即可,其他节点不需要。 您提到的通讯乱码我认为和匹配有一定关系的。