This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1042-Q1: VCC1侧使用1.8V供电时无法通信

Part Number: ISO1042-Q1
Other Parts Discussed in Thread: ISO1042

TI专家,您好。

最近我在使用ISO1042QDWVQ1做can通信时,参考数据手册,为了能直接连到1.8V的FPGA,在VCC1侧使用了1.8供电。但是实际电路无法正常通信,收发都不行。在FPGA和iso1042之间加一级电平转换,将FPGA的1.8V信号转为3.3V,ISO1042的VCC1使用3.3V供电后,能够实现can通信。VCC1和VCC2是供地的,没有隔离。我不太理解为什么会这样,ISO的手册上是明确注明可以使用1.8V系统的,为什么实际却不能正常工作?请指教,万分感谢。

我的设计如下: