Part Number: ISO1050
ISO1050在运行中,DSP接收信号正确,DSP的TX数据异常,更换IS1050的芯片后DSP的TX数据恢复正常。
1. ISO1050的RX损坏的话,应该是影响道ISO1050接收端的电平受到影响,而实际情况是电平任然是3.3V ,只是数据内容异常,这个情况是否合理?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO1050
ISO1050在运行中,DSP接收信号正确,DSP的TX数据异常,更换IS1050的芯片后DSP的TX数据恢复正常。
1. ISO1050的RX损坏的话,应该是影响道ISO1050接收端的电平受到影响,而实际情况是电平任然是3.3V ,只是数据内容异常,这个情况是否合理?
您好,
DSP连接ISO1050的TX和RX是吗?还是CAN接口?
如果DSP是连接的ISO1050 的TX和RX这端的话,“DSP接收信号正确”是指CAN总线传输过来的信号正常,“DSP的TX数据异常”是指DSP输出的TTL信号异常?或者说CAN总线正常,是ISO1050 的TX和RX这端出现了问题?

1. ISO1050的RX损坏的话,应该是影响道ISO1050接收端的电平受到影响,而实际情况是电平任然是3.3V ,只是数据内容异常,这个情况是否合理?
不太明白您为什么这样说,“DSP的TX数据异常”应该考虑ISO1050 的TX损坏使得DSP的输出异常,而不是考虑ISO1050 的RX损坏