This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7720-Q1: ISO7720 can't cooperate with TCAN1042

Part Number: ISO7720-Q1
Other Parts Discussed in Thread: ISO7720, ISO7721

I want to use ISO7720 to transfer CAN signal with TCAN1042, but the TX signal cannot transfer right signal while the MCU's CAN signal works well with TCAN1042, yellow:TX    blue:TCAN1042--VCC.why this happens?

  • 您好,我们可以直接使用中文沟通。

    ISO7721不能隔离CAN 差分信号,但是可以隔离数字信号TX,经过ISO7721后的TX信号波形有吗 ?可以附上看下。

    TX经过ISO7721的输入端以及输出端的波形,靠近引脚端测试。