Part Number: ISO7740
你好,
计划使用ISO7740进行最高42MHz时钟的信号隔离
VCC2的电源是浮动参考的3.3V电源
GND2连接模拟波形,在0-36V间波动,最大斜率不超过70V/us
ISO7740能否胜任?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.