This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7740: VCC2与GND2接浮动参考的3.3V电源可行吗?

Part Number: ISO7740


你好,

计划使用ISO7740进行最高42MHz时钟的信号隔离

VCC2的电源是浮动参考的3.3V电源

GND2连接模拟波形,在0-36V间波动,最大斜率不超过70V/us

ISO7740能否胜任?

  • 计划使用ISO7740进行最高42MHz时钟的信号隔离

    ISO7740支持最大dataa rate为100Mbps,即50Mhz,所以42Mhz的信号是支持的。

    GND2连接模拟波形,在0-36V间波动,最大斜率不超过70V/us

    GND2的是参考地电平,在0~36V之间波动,这是不允许的。VCCA最大能承受的电压也只能到6V,如果施加超过6V以上的电压也是会导致芯片损坏的。