This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO6741: 器件是否可以4个并行使用。

Part Number: ISO6741

器件是否可以4个并行使用?共用相同的总线,4个元器件的EN使能单独用一个IO。或能否更多于4个并机使用呢?   

目前我司发现不能并机使用,原因是IND引脚的电平在EN为低电平时,始终为2V左右的电压。