Part Number: SN74AHC1G08
请问SN74AHC1G08DRLR 输出是opendrain ,还是push pull的,在输出端可以加下拉电阻吗,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74AHC1G08
请问SN74AHC1G08DRLR 输出是opendrain ,还是push pull的,在输出端可以加下拉电阻吗,谢谢
Taylor
非常感谢你的回复
如下图,我们需要由SN74AHC1G08 输出3路信号,负载都是高阻输入的,包括
1)通过背板给2个主控卡cpld提供输入,设备要求默认cpld的输入默认为低,由于对端板子已经做好,只能在SN74AHC1G08这边默认做下拉了
2)给本地LED提供控制信号,控制一只NMOS,默认要关断,因此,也需要下拉
如果不加下拉,电路功能上可能会有问题,请帮忙看看,下图是否可以,谢谢