Other Parts Discussed in Thread: TXS02612, TXS0206
使用一路的TXS02612可以替换TXS0206吗?因为TXS0206的封装不是很适合,故使用TXS02612的一路代替TXS0206,或者有推荐QFN封装的高速SDIO、SD、EMMC电平转换芯片吗?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在VCCA = 1.8 V,VCCB = 3.3 V的情况下,我可以使用TXS02612的其中一个单通道实现高达120Mhz的数据吗?我看见数据手册中是最高可以达到这个传输速度。 谢谢!
您好,VCCA = 1.8 V,VCCB = 3.3 V时候的data rate最高为120Mbps,即为60Mhz。
如果您的应用为120Mhz的话,那就是240Mbps。 是不能够支持的。