This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TXS0108E 这类器件 VCCA 和 VCCB 的电平能不能相同。比如同为3.3VDC
1:应用,两颗芯片之间同为 3.3VDC电平,但是希望增强芯片的驱动能力所以添加 TXS0108E这个芯片。那VCCA 和 VCCB 的电平能不能相同?
2:备注,数据方向是双向的。
您好,
可以的,VCCA 引脚可 接受 1.2V 到 3.6V 范围内的任意电源电压。B 端口跟 踪 VCCB 引脚的电源电压。VCCB 引脚可接受 1.65V 到 5.5V 范围内的任意电源电压。但是需VCCA ≤ VCCB。
多谢。