This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

器件推荐



Hi

目前客户有一个需求:

MCU有个供电引脚,我们需要控制该引脚接地和接电源,使用某个功能时需要接1.8V200mA)的电源,不使用时想要接地。根据该需求希望您帮忙推荐一颗符合这样逻辑的器件,需要是汽车级的,请问这种算哪类器件,谢谢!

  • 您好, 按照您的描述,SPDT符合要求,但是这里需要切换的是电源和GND,但是200mA的电流太大了,逻辑器件的最大source后sink的电流也没有这么大呢。 

    可以看下power版块的电源开关是否有满足要求的。