Part Number: SN74LVC1G123
1、当前 A 接GND ,B连接到了一个8M的有源晶振,CLR接在VCC(5V)上。示波器测到7号引脚是有锯齿波的。R的阻值为1K ; C 的阻值为100pF,但是输出只有高电平。电路参考了手册中第13页的推荐电路对输入做了改动。
2、如何计算Tw的时间,RC的取值有计算公式吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC1G123
1、当前 A 接GND ,B连接到了一个8M的有源晶振,CLR接在VCC(5V)上。示波器测到7号引脚是有锯齿波的。R的阻值为1K ; C 的阻值为100pF,但是输出只有高电平。电路参考了手册中第13页的推荐电路对输入做了改动。
2、如何计算Tw的时间,RC的取值有计算公式吗?
您好,datasheet中Figure11-13给出了不同电压下,脉冲宽度VS电容的曲线,根据需要的脉冲宽度,去查询对应的R和C的值大小。
您的应用VCC=5V的话,参考FIgure13.如何选择Rl,还是根据想得到的脉冲宽度,然后沿着tW的去找R和C的交叉值,哪个值对应曲线中比较方便,就选哪个RL,然后再对应查到C的值大小。举个例子,比如想得到10^6ns的tW脉宽,可以看到选择Rl=100K时,C大约正好在10^4pF这里取值比较方便。