This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC14: 关于多路逻辑芯片的规格书内输出电流能力问题

Part Number: SN74HC14


以标题的6路施密特触发反相器为例,规格书Absolute Maximum Ratings表内的:

Iik Input clamp current(2) VI < 0 or VI > VCC ±20 mA

Iok Output clamp current(2) VO < 0 ±20 mA

IO Continuous output current VO = 0 to VCC ±25 mA

     Continuous current through VCC or GND ±50 mA

以上内容针对的是每路反相电路(即每路都可同时输出或输入20mA电流),还是芯片所有6路的总和?

  • 您好,输入输出钳位电流都是指的每个通道的钳位电流. 但是Continuous current through VCC or GND ±50 mA 这里指的是toal current, 也就是说如果所有的通道同时使能的话最大不能超过这个值.  所以,如果6个通道同时输出的话,最大电流不能超过50/6=8.33mA.