This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC14: 指示灯无法完全熄灭

Part Number: SN74HC14
您好以下是物料测试情况,请分析下原因,谢谢
测试条件:通过稳压电源在110VCS(Q-1)对110VG(X1-DBZ26)加入77~110V直流电压信号,面板指示灯1A-4B亮,当电压低于60V时,面板指示灯1A-4B灭
异常情况:面板4A指示灯无法完全熄灭,测量芯片1脚与地,存在1V左右的电压
排查情况:1、更换NXP品牌的物料,故障消失 
                  2、更换TI原厂提供样品,故障消失
                  3、更换2115批次芯片,故障消失
另外:没问题的两个前面丝印是竖线,有问题批次2117+货前面是个小圆坑,看有什么区别。