This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0108: 使用LSF0108 在50MHz频率下波形失真较大

Part Number: LSF0108


LSF0108RKSR做信号的电平转换器,效果不太理想,在50MHz频率下波形失真较大. 请问有解决方案吗?或者是有其他型号推荐!!

要求:

1.时钟频率最高达208MHz

2.支持1.8V3.3V电平转换,双向数据传输

  • 您好,

    LSF0108支持的数据速率与容性负载有很大关系,在不超过 30pF 的容性负载条件下支持最高达 100MHz 的 上行转换和超过 100MHz 的下行转换,在 50pF 的 容性负载条件下支持高达 40MHz 的上行/下行转换。在50MHz频率下波形失真较大,应该是容性负载太大了

    您具体是对什么信号进行电平转换?还是需要8 bits的吗?