Part Number: TXS0104E-Q1
Other Parts Discussed in Thread: SN74AXC4T774
使用贵司的TXS0104E-Q1芯片做3.3-5v的SPI转换,电路如下:

SPI通信速率1M左右,奇怪的是,B1端口的SCLK输出时钟波形如下,A1端口输入正常,其他B端口输出也正常是5V逻辑

将B端口的负载去掉之后,直接测量发现只有B1端口是3.3v逻辑,请问这个是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXS0104E-Q1
Other Parts Discussed in Thread: SN74AXC4T774
使用贵司的TXS0104E-Q1芯片做3.3-5v的SPI转换,电路如下:

SPI通信速率1M左右,奇怪的是,B1端口的SCLK输出时钟波形如下,A1端口输入正常,其他B端口输出也正常是5V逻辑

将B端口的负载去掉之后,直接测量发现只有B1端口是3.3v逻辑,请问这个是什么原因?
您好,
TXS电平转换器适用于速度和负载电容不太大,且集成上拉电阻器的场合。您可以确认一下您描述的“SPI通信速率1M左右”,是指的1Mbps还是1MHZ ?如果是1MHZ则可能是速率太大的缘故。
B1信号线走线长不长?后端负载是什么负载?如果走线太长就会形成较大的寄生电容。
A1是什么驱动接口?如果是OD驱动,则需要接上拉电阻。
一般来说,SPI的最佳解决方案是具有适当缓冲区的转换器,即SN74AXC4T774。
关于B1端口是3.3v逻辑,您测得的波形是什么样的?测试时VCCB供电电压是多少?