This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXU0304-Q1: 用于4l ane SPI电压转换

Part Number: TXU0304-Q1
Other Parts Discussed in Thread: SN74AXC4T774-Q1

TXU0304-Q1没有VCCA≤ VCCB的限制对吗?

一个10MHz的SPI 1.8V 转3.3V的应用 ,SN74AXC4T774-Q1和TXU0304-Q1是否更推荐TXU?

感谢