Part Number: LSF0108-Q1
电路中有多个IIC通信,打算用LSF0108-Q1的EN脚控制选择开通,节省IO。如下图VREFA是1.8V,VREFB是3.3V,EN脚接IO脚加1.8V的上拉。
1,这是设计跟手册上有出入,我这样设计是否有问题?我第一版设计是EN脚加VREFB_3.3V的上拉但是A端输出有2.2V的电压,把VREFA的1.8V也拉到2.2V了,影响了通信电平。下图设计是第二版


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LSF0108-Q1
电路中有多个IIC通信,打算用LSF0108-Q1的EN脚控制选择开通,节省IO。如下图VREFA是1.8V,VREFB是3.3V,EN脚接IO脚加1.8V的上拉。
1,这是设计跟手册上有出入,我这样设计是否有问题?我第一版设计是EN脚加VREFB_3.3V的上拉但是A端输出有2.2V的电压,把VREFA的1.8V也拉到2.2V了,影响了通信电平。下图设计是第二版


您好,
不可以这样接,LSF 内部Vref_B与Vref_A之间是一个FET,需要使用200KΩ是电阻限流,如下截图所示:

控制EN管脚的驱动电路需要是OD输出的,且EN管脚连接到Vref_B,然后通过200KΩ电阻上拉到VCCA,如下截图所示:

LSF系列的电平转换工作原理,请观看下面链接视频:
https://training.ti.com/using-enable-pin-lsf-family?context=1134826-1139264-1134791
您的意思是说VREFB端电压由3.3V变为2.7V了吗?
Vref_A、Vref_B电压是怎样产生的,请注意,在正常运行期间,电流将流入A侧电源,如我上面截图所示,因此,请确保您的设计的Vref_B能够处理这种电流。
上述描述A端电压是1.91V,是指A侧I/O口的输出电压吗?也就是说是芯片工作在降压转换过程中输出异常?
1,如图A点电压是3.3V,B点电压是2.7V,C点电压是1.8V
2,A测1.8V电源是AMS1117-1.8产生,B测3.3V电源是DC-DC芯片产生设计为最大电流1A
3,电阻换成1M输出1.91V是A测的I/O口输出的电压(3-9脚都是输出1.91V),如果是200K电阻A测I/O电压为1.97V
A点电压是3.3V,B点电压是2.7V,C点电压是1.8V,都是实际测量值吗?
我感觉应该是LDO AMS1117-1.8的原因,因为其输出端口内部是电阻网络,与200K电阻形成分压网络,造成A侧端口电压异常。您可以尝试换其他非线性电源供1.8V电吗?以验证是否与LDO有关。
1,那几个点的电压都是实际测量的值
2,今天用新的IC在面包板上测试,3.3V和1.8V都是用的稳压电源给的,A测I/O输出还是1.9V多点
3,可是我把1.8V调到1.7V之后,测量A测I/O的输出是1.8V左右,我不清楚是不是芯片的VREFA端电压就是给1.7V,A端电压就输出1.8V呢?
A测加入1.8V的上拉,测量A测IO输出电压为1.8V,
1,有没有详细的芯片内部图纸,我想看一下,因为我感觉A测加上拉之后高电平是1.8V了,但是低电平跟不加上拉的有50MV左右的电压差?
2,是不是A侧IO和B侧IO都要加对应VREF的上拉呢?
上述视频中有显示芯片的内部电路图;
电压降电平转换,如果接上拉电阻的话,接收端低电平电压会比LSF输入端高一点;如果进入接收端的漏电流大于1uA,那么接收端需要接上拉电阻。具体见下面视频原理分析:
https://training.ti.com/down-translation-lsf-family?context=1134826-1139264-1134793