This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108: OE端下拉电阻和驱动电流问题

Part Number: TXB0108


目标:使用TXB0108实现1.8V到3.3V的电平转换。

详情:驱动器(FPGA)输出使能信号到OE端,FPGA约束1.8V,实测OE端电压只有0.99V

问题:手册要求下拉电阻至少50K,并且取决于驱动器电流大小。而目前OE端只用了10K的下拉电阻,FPGA电流驱动8mA,是否会是这两项参数的问题?

  • 您好,

    数据手册中描述的上下拉电阻至少50KΩ,指的是TXB的 I/O 口,也就是A1~A8和B1~B8,并不是OE管脚;

    您这里连接OE的FPGA接口类型是不是配置为了pullup类型?应该是这里设置的上拉与您外接的下拉电阻形成了分压电路,OE电压也就是下拉电阻的分压。您这里是否可以配置为推挽输出?再看OE电压是否正常

  • 由于您长时间未回复,我认为您的问题已解决,若仍有疑问,您还可以继续回复帖子