TXB0108PWR 用于SPI电平转换,实现3.3V主控端到3.0V外设端电平转换。外设CLK的范围是2MHZ-20MHZ,请问TXB0108PWR 能否支持20Mhz的电平转换?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您需要3.3V转3V的电平转换吗?您可以下3.3V的IO电平阈值是不是和3V的阈值相同,从而确认下是否能直接接,不需要电平转换呢?
我们常用的电压是1.2V,1.5V,1.8V,2.5V,3.3V或者5V的电平转换。
那么对于TXB0108来说,实现不同的电平转换,能够支持的最大速率也是不一样的,如果VCCA=3.3V,VCCB=5V的话则最大能支持100Mbps=50Mhz。
具体可以参考数据手册中的P8的电气参数。