目标波形:

经过TXB0108之后的波形:

请问出现这样的波形是怎么回事?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有2种方法可以尝试用来去解决:
1、在信号线上串联电阻,以增加驱动电容的能力,但是形成的RC充电时间常数会影响数据速率,鉴于您使用的速率是100KHZ,您可以尝试一下;
2、使用TXS0108替换TXB0108, 它们是P2P兼容的,但是对于较大的容性负载,TXS0108也不一定可行;
如果这两种方法都不能解决问题,那只能考虑其他驱动能力更强的电平转换IC了,对于选择IC,下面FAQ可能对您有帮助:
串联电阻在TXB0108的输出端连接,这样与后端信号走线上的寄生电容形成RC;
我明白PCB板已经设计好了,所以让您尝试前2种方法,如果前2种方法不能解决问题,只能改版设计,重新选型其他驱动能力更强的电平转换IC。这时需要您提供需要电平转换的信号方向是单向还是双向,信号类型或信号速率,驱动能力等设计要求
我看到您重新发了一个帖子,我将在您下面新帖中回复您,这个帖子我先关了
https://e2echina.ti.com/support/logic/f/logic-forum/272744/txb0108