Part Number: SN74LV1T08
hello TI
SN74LV1T08DBVRG4 相关咨询
此与门逻辑芯片是否支持 1.8V VCC供电,
逻辑输入A或B 用3.3V电平,实现3.3V到1.8V的下行转换
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LV1T08
hello TI
SN74LV1T08DBVRG4 相关咨询
此与门逻辑芯片是否支持 1.8V VCC供电,
逻辑输入A或B 用3.3V电平,实现3.3V到1.8V的下行转换
谢谢!
您好,可以支持的,当VCC=1.8V时,输入是能承受0~5.5V输入,输出参考VCC电压
因此可以实现降压电平转换,比如VCC=1.8V, 可以实现2.5V,3.3V或者5V到1.8V的降压电平转换。