Part Number: SN74LVC2244A
你好:
根据SN74LVC2244A规格书可知,该BUFFER电源电压为3.3V时最大输入信号电平为6.5V。目前我们有一个错误的设计将该芯片的输入电压设计为了12V,并且可以正常工作。可以从芯片内部原理上解释下为什么12V也是可以承受的吗?
感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC2244A
你好:
根据SN74LVC2244A规格书可知,该BUFFER电源电压为3.3V时最大输入信号电平为6.5V。目前我们有一个错误的设计将该芯片的输入电压设计为了12V,并且可以正常工作。可以从芯片内部原理上解释下为什么12V也是可以承受的吗?
感谢!
您好,首先这款器件输入时5.5V tolerance,即使工作在3.3V。
输入最大电压是不能超过6.5V的,如果超过了6.5V有可能噪声器件永久性损坏,所以我们在使用时需要参考Recommend Electrical Characteristics,而不是最大值,这是针对所有TI芯片的电气特性。像您提到输入12V远远超过了最大6.5V的耐压值,这个也是不允许的。但是您提到目前看起来是能正常工作的,但是绝对不能保证能长久稳定工作,至于它的功能也是无法参照数据手册的。 建议按照芯片的datasheet去使用,能保证它的最优性能。