Other Parts Discussed in Thread: TXB0108,
您好,
目前我由如下接口需要做电平转换,从1.8V 转换到3.3v
接口有
1. IIC
2. SPI
3. UART
4. GPIO
但是在不知道TXS0108E与txb0108这两个物料应该选择?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,TXB010x系列的不适合用于I2C这类开漏输出的应用。

所以建议选用TXS010x系列的,既能应用于push pull也能用于open drain的器件:
您好,如上面我附上的datasheet截图,可以上拉,但要求50Kohm以上来保证它不与TXB0108的输出驱动抗衡。换句话说,上拉是允许的,但是起不到作用。
如果改成强上拉,则输出一直保持高电平,这是TXBxx系列不适合用于上下拉应用的open drain应用。
如果I2C的话,建议使用TXSxx系列。
另外也要注意,TXS和TXB的驱动能力很弱,只有uA级,如果对驱动能力有要求的话,建议还是使用带有方向控制位的电平转换器件。