Part Number: SN74AHCT245
DSP280049 PWM低电平最高0.4V,高电平最低2.64V,那么当280049 PWM接SN74AHCT245后,SN74AHCT245输出电压是多少呢?是否假如高电平2.64V,接SN74AHCT245输出2.64V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74AHCT245
DSP280049 PWM低电平最高0.4V,高电平最低2.64V,那么当280049 PWM接SN74AHCT245后,SN74AHCT245输出电压是多少呢?是否假如高电平2.64V,接SN74AHCT245输出2.64V?
您好, SN74AHCT245其实是一款总线收发器,输入和输出幅值是相同的,比如5V CMOS输入,还是5VCMOS输出。
但是由于5V TTL和3.3V LVTTL电平的阈值是相同的,所以当输入3.3V LVTTL时输出仍是5V,相当于实现3.3V到5V的升压电平转换。
那对于您提到的PWM信号,Voh(min)=2.64V,Vol(max)=0.4V 也是符合3.3V LVTTL的阈值(Vih(min)=2V,Vil(max)=0.8V)的,所以相当于3.3V LVTTL输入,输出应该是5V的。您可以参考数据手册10.1 Application Information的应用部分: