CD74HC393数据表的几个截图
问题1:如中间图所示,如果计数到HHHH,不进行人为复位,下一个时钟信号来了后,会自动变成0000吗?还是说必须把最高位给拉到复位脚,强制变0000?
问题2:这个计数器是下边沿触发,我想给它供电到6V,保证有最大的工作频率,但是进去的是27MHz的正弦信号,峰峰值5V,中心值3V,可以识别吗?可能存在什么问题?
问题3:有什么可以参考的应用电路推荐的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CD74HC393数据表的几个截图
问题1:如中间图所示,如果计数到HHHH,不进行人为复位,下一个时钟信号来了后,会自动变成0000吗?还是说必须把最高位给拉到复位脚,强制变0000?
问题2:这个计数器是下边沿触发,我想给它供电到6V,保证有最大的工作频率,但是进去的是27MHz的正弦信号,峰峰值5V,中心值3V,可以识别吗?可能存在什么问题?
问题3:有什么可以参考的应用电路推荐的吗?
感谢回复。
如你在datasheet中得这个截图,所以我计划工作电压给6V,数据手册中不是标注MIN 最差可保证工作频率35MHz,脉冲宽度14ns,看起来可以。
问题是这个计数器是下降沿触发,正弦信号的变化率不知道它能识别不?
如果不行,前面想加一级非门,电平触发翻转,这个高低状态门限很大,出来的绝对就是方波,计数器应该就可以很好识别了。这个非门有推荐的吗?
工作电压5V,输入正弦峰峰值不超过5V,中心保证在2.5V.频率还是27MHz.
如你在datasheet中得这个截图,所以我计划工作电压给6V,数据手册中不是标注MIN 最差可保证工作频率35MHz,脉冲宽度14ns,看起来可以。
脉冲宽度14ns是在工作环境温度25℃时的参数,设备不可能总是工作在25℃,因此您至少需要看-40℃ ~ 85℃这个温度范围的参数。
咱们先看脉冲宽度是否满足要求:
可以识别的高电平至少是4.2V,如果是27MHZ正弦波,那么到达4.2V的时间可以根据1.7V=2.5Vsin(2π*f*t)来计算。2πft=42.84364°--> t=8.8ns,27MHZ的半周期时间是18.5ns,那么高电平时间是18.5ns-2*8.8ns=0.9ns<17ns,因此是不满足要求的。
关于这个公式:1.7V=2.5Vsin(2π*f*t),正弦波中心值是2.5V,算的是从2.5V升至4.2V(4.2-2.5=1.7V)的时间。这里是不是没有计算错?