Part Number: SN74F161A
这块有个应用问题,我有一个27MHZ±1K的方波信号,需要知道确切值,想送入单片机测试频率,这个信号对单片机来讲太快了,所以想用161来降低频率,如果这个27M信号从CLK输入,ENP 与ENT一直保持高,是不是QA的输出一直是CLK的1/2频率,QB一直是CLK的1/4倍频率。
有点着急,忘各位给个解答,感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74F161A
这块有个应用问题,我有一个27MHZ±1K的方波信号,需要知道确切值,想送入单片机测试频率,这个信号对单片机来讲太快了,所以想用161来降低频率,如果这个27M信号从CLK输入,ENP 与ENT一直保持高,是不是QA的输出一直是CLK的1/2频率,QB一直是CLK的1/4倍频率。
有点着急,忘各位给个解答,感谢。
是的。上图是设置的预置值为二进制12,所以看到输出为二进制12,13,14,15,0,1,2,然后发出inhibit指令。
如果预置值为0的话,在每个clock的上升沿发生变化,输出依次为0000,0001,0010,0011,0100,0101........1111
可以看到QA的输出频率是1/2 CLK,QB的输出频率为1/4CLK.