Other Parts Discussed in Thread: TXS0102, , SN74HC245, SN74HC175
Hi,TI
请问缓冲器像74HC245、电平转换芯片像TXS0102所能支持的最大频率如何根据规格书去算?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
您可以根据下面FAQ去计算:
[FAQ] What is the output transition rate for a logic device?
关于TXS0102,datasheet中给出了一些data rate参数,如下截图,测试负载是15pF//1MΩ
1. FAQ里面计算出来的是tLH和tHL。如果传输数据信号的话,比如SPI,时钟速率要求20MHz。而这个时钟实际上是数字量。
数字量除了tLH、tHL外还会有tw、tpd等。那么这个数字量能传输的时钟频率能支持到多少?请问这个是怎么算的?
2. 如上提了个时钟频率单位为Hz,而像TXS0102里面会提到速率单位为bps。
TXS0102在3.3V的情况下,推挽模式的速率为24Mbps,那么请问这个能够支持的最大频率是多少?24MHz还是会比这个更高?
谢谢!
1、抱歉,附错链接了,数据速率应该看这个FAQ:
如下截图所示,SN74HC245A没有时钟输入,它属于 transceiver产品,datasheet中没有给出其数据速率,但是它可以根据同一逻辑系列中的时钟设备,估计最大工作频率。比如同一列的SN74HC175,它在VCC=4.5V时,fmax=25MHZ,那么在同样供电电压下SN74HC245也可以工作在25MHZ。
2、24Mbps=12MHZ
bps是bit per second,频率是一个周期包含2位,因此是2倍关系。