Other Parts Discussed in Thread: TXS0108E, TXS0206, TXS0206A
参考AM335x starter kit开发板,将SDIO1接到LBEE5ZSTNC-523m(WL1271L)模块。
在设计中将AM335x的MMC1 IO电平置为3.3V,因此需要用到电平转换芯片。
请问如图所示,将SDIO的数据线、命令线、时钟线用一个TXS0108E作电平转换,是否可以?另外,外接的上拉电阻是否正确?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zhaohui,
你用下滑红线标注的部分正说明SDIO的接口需要主设备提供上拉,开漏结构的逻辑接口需要上拉才能正常工作,如I2C。
所以上拉后的速率没有问题。
Hi Zhaohui,
你在电路上做了上拉处理,所以速率没有问题。
我看了一下SDIO的标准, TXS0108E的问题在于CMD信号。SDIO在初始化时为了非常准确和稳定的同步使用的是OD模式,然后在数据传输时切换到上拉模式已达到更高的速率。
鉴于SDIO特殊的工作模式,你可以看一下TXS0206,这个应该更适合你的应用。
您好,,我的应用是:A侧作为SPI的SCK输入,A侧1.8V电压,B侧3.3V。SCK引脚是否支持下拉电阻1kΩ。在Datasheet第21页有这样的描述:
• An external pull-down resistor decreases the output VOH and VOL. Use Equation 1 to calculate the VOH as a
result of an external pull-down resistor.
VOH = VCCx × RPD / (RPD + 4 kΩ)
若下拉1K电阻,输入高电平就是1.8/5=0.36V,那么A侧输入0.36V就是高电平了,低于0.36V就是低电平,可以这么理解吗???
作为SPI通信,若想SCK默认电平为低电压,您的推荐硬件电路该怎么设计呢???
期待您的回答,,多谢!!!