This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We did not find the output resistance of SN74AUC74 and SN74AUC1G74 in their datasheet. Please help us confirm the value. Thanks a lot.
The output impedance can be derived from the VOx/IOx values .See FAQ:, we could found that the output impedance will depend on the supply voltage. For example, VCC=3V,Voh=2.3V, Ioh=24mA , then Rout= (Vcc-VOH)/IOH=(2-2.3)/0.024=29.167ohm.
Thanks. We shall use SN74AUC74 and SN74AUC1G74 with VCC=2.5 V. But there is no parameter that is related to VCC=2.5 V. Could you help us to find the paramater?
I am so sorry we didn't have the detailed Voh and Ioh with VCC=2.5V, but we could calculate approximately:
when VCC=2.3V. Voh=1.8V which is about 78%VCC, when VCC=1.65V, Voh=1.2V which is about 73%VCC. If we used 78%VCC, VCC=2.5V, then Voh is about 1.95V or 80%VCC is 2V, similarly, the output current is higher than VCC=2.3V, we could use =10mA, so we could calculate the approximate value:
Ro=(2.5-1.95)/0.01=55ohm.
That it to say, the output impedance is about 55ohm with 2.5V power supply, but unfortunately, we didn't find the specified value about this, but I think it could use 55ohm to evaluate the IC function.