Part Number: TXS0108E

Module的GPIO在开机过程有一个输出3V高电平(持续约2s),然后才恢复输出变成1.8V
查看资料TSX0108E的输入端口的绝对最大值在A端口供电1.8V时,A端口最大的输入只能到2.3V

想咨询一下按照以上原理图设计,TXS0108E芯片的使用是否有风险?能帮解答一下吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

您好,我还想请教您一下该链接下的“逻辑器件的输入电压可以高于电源电压”是否适用于TXS0108E芯片呢?如果适用的话就不用去控制OE管脚了,GPIO的3V也没有达到4.6V不会对于芯片有所损害。