Hi Expert,
We want to connect two 3.3V MACs without going through PHY IC. We are planning to have a 1000Mbit/s connection via these RGMII interfaces.
We want to use SN74AXC8T245 as a buffer between the two MAC.
Is the timing (delay) of the SN74AXC8T245 with in the specs for a RGMII Bus?
Is the propagation delay consistent for each channel?
Thanks.