This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
我在设计中使用了TXS0108E用于FPGA加载Flash的开关,VCCA和VCCB均为同一个1.8V,使能实测上电后也立即到1.8V,但是FPGA加载Flash未能成功,QSPI的片选,时钟,复位,以及4路IO均通过TXS0108E;尝试过跳过TXS0108E飞线直接连接可以顺利加载,实测加载时的QSPI时钟频率为25Mhz;请问有什么办法在不更换TXS0108E的情况下,实现QSPI信号的顺利通过吗?
您好,您有测试四路信号经过TXS0108E之后的输出波形吗?在靠近TXS0108E的输出端用示波器测试下,是否能正常输出? 可以将波形附上看下。
另外,麻烦将TXS0108E的电路也附上。